Post Go back to editing

The Output of HMC836 Drop 7dBM After 2-3 Years Intermittent Working.

Thread Summary

The user experiences a significant drop in output power from the HMC836 Local Oscillator from 2dBm to -5dBm over a few years. The final answer suggests checking if the absolute max ratings or ESD limits were exceeded, and recommends contacting the local sales channel for return options. No specific URLs or additional clarifications are included.
AI Generated Content

Hi, once I use HMC836 as a Local oscillator output 3.6GHz. The circuit schematic is designed following the evaluation board. There is no problem in the previous two years, and the output power is about 2dBm. After a few years, they are generally reduced to -5dBm. The output power requirements can't reached, and the overall circuit failure appears.

Do you have received any feedback in this regard. Do you have any repair measures besides replacing a new HMC836 chip? Thank you!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.