Hi support,
I cannot find the HMC553ALC3B model on ADIsimRF v2.0.0.16, deployment 1.0.0.13, databese 2.00.014.
How can I simule the component in a RX downconversion chain (fRF=9400MHz, fLO=7500MHz)?
Thank you
HMC553ALC3B
Production
The HMC553ALC3B is a general-purpose, double-balanced,
gallium arsenide (GaAs), monolithic microwave integrated
circuit (MMIC) mixer housed in a leadless...
Datasheet
HMC553ALC3B on Analog.com
Hi support,
I cannot find the HMC553ALC3B model on ADIsimRF v2.0.0.16, deployment 1.0.0.13, databese 2.00.014.
How can I simule the component in a RX downconversion chain (fRF=9400MHz, fLO=7500MHz)?
Thank you
Hi, you have a couple of options. You could pick a similar part such as HMC554 which has a minimum input frequency of 10 GHz. If you select this part and type in a frequency of 9400 MHz, the tool will accept this (it will give you a warning message) and will use the data it has at 10 GHz. The second option is to create a custom part. The process for doing this is described in one of the help menu items. Make sure you are in receive mode before you start the process (so that you can save the device as a "Mixer (Rx)"

Ok, I did my own part as you suggest.
My curiosity, why does ADIsimRF not invole the HMC553ALC3B model?
No particular reason. We have hundreds of parts and try to focus our efforts on modelling the newer parts. I can add HMC553 to the list of devices for the next release but that won't launch for a few months.
Thank you enash!