Hello.I have two questions. please tell me.
Question1:Can you provide the maximum input power to the RF terminal of the following products?
Or can I use it even if +10dBm is input to the RF terminal without any damage?
・HMC-MDB277
・HMC-MDB218
・HMC-MDB169
Question2:The HMC-MDB277 can be used between 70GHz and 90GHz. Is there any reference characteristics for 60GHz-90GHz?
Best regards.