Post Go back to editing

HMC625B for low frequency application

Hi, 

I would like to know if the HMC625B can be used from 10kHz. I planed to use this part in a broadband transmitter from 10Khz to 1Ghz. The title of the datasheet mentioned the frequency range from DC to 5GHz, but according to the curves in datasheet the Gain goes down to about 5dB near DC and the input/output return loss is so bad at these low frequencies. So how could I use this part in low frequencies like 10kHz, 100KHz, etc ? Do I need to use extra matching circuits or others modifications ? Or do you have other VGA parts to recommend ? ADL5331 can be used in theses low frequencies ?

Thanks in advances,

Best regards,

Xl 

Parents Reply Children
No Data