Post Go back to editing

Power-up/Power-down Sequence VSS VDD Vctrl HMC649A Digital Phase Shifter

Thread Summary

The user asked about the correct power-up and power-down sequence for the HMC649A Digital Phase Shifter, specifically if the 6-bit V-CTRL can remain on during power-off. The final answer from ADI tech support recommends turning on VDD and VSS simultaneously with control inputs initially at ground or floating, and warns against having digital inputs at logic 1 while VDD and VSS are at 0V.
AI Generated Content

Hi, 

What is the recommended Power-up/Power-down Sequence of VSS, VDD, and 6-bit +ve V-CTRL signals for HMC649A Digital Phase Shifter?

Is the following sequencing correct ?

Power-On: VSS, VDD, and Vctrl 

Power-Off: Vctrl, VDD, and VSS 

Could this device (internal RF Switches or phase shifters) get damaged, if 6-bit V-Ctrl remains ON, while VDD is OFF?   

TIA

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.