HMC767
Last Time Buy
The HMC767LP6CE is a fully functioned Fractional-N Phase-Locked-Loop (PLL) Frequency Synthesizer with an integrated Voltage Controlled Oscillator (VCO...
Datasheet
HMC767 on Analog.com
Hi,
I'm having difficulty programming the HMC767 and I've found some related issues on the EngineerZone but so far the fixes haven't helped in my case. I'm trying to setup the PLL in fractional mode, however I'm meeting with limited success. The register values I use for initialization are below. They're similar to the default configuration for the PLL from the HMC PLL evaluation example, however I'm using an RDiv value of 2 and a different integer value.
0x01 0x000002
0x02 0x000002
0x03 0x00005C
0x04 0x000000
0x05 0x000001
0x06 0x00F51E
0x07 0x00085D
0x08 0x036FFF
0x09 0x5B7FFF
0x0A 0x000000
0x0B 0x01E070
0x0C 0x000019
0x0D 0x000000
0x0E 0x000000
0x0F 0x000001
At some time after powering the device (it can be several minutes) I'm sending all the default registers to the device using a Beaglebone Black. The SPI driver on the Beaglebone asserts the SEN line well before the first SCK cycle, so the device should be put in HMC mode. I can also read back these values and they contain what was written.
The first problem is that the after the PLL is initialized, it puts out a very strong ~8.91 GHz signal no matter what I set the integer or fractional registers to. Since I am changing the RDiv register, I toggle 0x07[20]. I'm also writing the integer register then the fractional register at the end of the initialization, then toggling the SPI trigger register (0x0E). Is there a particular order that I should be writing the default values in or another register/value I should be looking into?
On a related note, I would also like to change the frequency of the PLL. When I attempt to do this, I am writing the integer register first, then the fractional register, then toggling the SPI trigger register, however the PLL frequency doesn't change. Is there another register or sequence of registers that I should be writing to change the frequency?
In regards to the hardware setup, I am using a custom board however the schematic and passive values (apart from the loop filter which was changed to a 4-pole design) are identical to the evaluation module.
Thanks,
Tyler
Hey,
I just wanted to say thanks for meeting to discuss the problem! We are now able to program the HMC767 correctly. The main issue was that we switched from an active loop filter design to a passive one but didn't change the PFDInv bit in the PD register (0x0B) from 1 to 0.
Thanks again,
Tyler
Hey,
I just wanted to say thanks for meeting to discuss the problem! We are now able to program the HMC767 correctly. The main issue was that we switched from an active loop filter design to a passive one but didn't change the PFDInv bit in the PD register (0x0B) from 1 to 0.
Thanks again,
Tyler