ADL5561
Recommended for New Designs
The ADL5561 is a high performance differential amplifier optimized for RF and IF applications. The amplifier offers low noise of 2.1 nV/√Hz and excellent...
Datasheet
ADL5561 on Analog.com
In the specification section for 140Mhz OIP3 is +39dBm for AV = 15.5 dB, RL = 200 Ω, VOUT = 2 V p-p composite (2 MHz spacing), but figure 13 shows another results. Why it is so ?
In my point of view 2 V p-p composite (RL=200Ohm diff or not ?) = 4dBm per tone ? And what the difference between 2 V p-p composite and 2 V p-p envelope?

Hi,
For the ADL5561 and similar parts, because they are specified with a 200-ohm load, the dBm specifications are with reference to this impedance and not 50-ohms.
Yes, composite is the same as envelope. So 2Vpp composite is 1Vpp/tone for a two-tone sinewave test
This does make the number for OIP3 in the specification table look a little conservative.
OIP3 = 39dBm
IMD3 = -96dBc
If the numbers above are correct, then OIP3 from IMD3 would be
-2dBm(200) + 96/2 = 46dBm(200) vs 39dBm specified in the specification table.
IMD3 = -96dBc looks reasonable from Figure 12, but I cannot figure out how 39dBm was arrived at.
Warm Regards,
Rachana
Hi,
For the ADL5561 and similar parts, because they are specified with a 200-ohm load, the dBm specifications are with reference to this impedance and not 50-ohms.
Yes, composite is the same as envelope. So 2Vpp composite is 1Vpp/tone for a two-tone sinewave test
This does make the number for OIP3 in the specification table look a little conservative.
OIP3 = 39dBm
IMD3 = -96dBc
If the numbers above are correct, then OIP3 from IMD3 would be
-2dBm(200) + 96/2 = 46dBm(200) vs 39dBm specified in the specification table.
IMD3 = -96dBc looks reasonable from Figure 12, but I cannot figure out how 39dBm was arrived at.
Warm Regards,
Rachana
Thank you for your explanation!