Post Go back to editing

ADI simPLL Op-Amp parameter for active filter

Thread Summary

The user reported discrepancies in peak amplitude and op-amp oscillation when using the OP184 with a 1MHz loop filter in the ADF4159 EVB, which are not accounted for in ADIsimPLL. The support engineer acknowledged the lack of op-amp GBW modelling in ADIsimPLL and confirmed that this feature is being considered for future releases. No specific workaround was provided.
AI Generated Content

SimPLL doesn't take account into phase & BW info. of Op-Amp for active filter. ADF4159 EVB uses OP184 which is 4MHz BW. When we set around 1MHz loop-filter,  it causes the peak amplitude discrepancy between simulation and measurement at 1MHz offset, and in addition, op-amp oscillates and VCO is modulated, like FM signal at certain Charge pump current condition.

Could you add an option on simPLL that takes care about op-amp parameters?

PDFPDF

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.