AD8343
Production
The AD8343 is a high-performance broadband active mixer. With wide bandwidth on all ports and very low intermodulation distortion, the AD8343 is well suited...
Datasheet
AD8343 on Analog.com
AD8220
Production
The AD8220 is the first single-supply, JFET input instrumentation amplifier available in an MSOP package. Designed to meet the needs of high performance...
Datasheet
AD8220 on Analog.com
Dear community,
I wish to make a phase detection of two sinus signals. I am a beginner in the field and seeking for some advices.
My setup would be the following:
- DDS (i think of using the AD5932) to deliver my reference signal. I want to have a frequency range variable but the limit of the AD8343 is already enough for my application,
- This signal goes thought my DUT. Since this one is tied to the ground, I am measuring the current flowing thought a reference and transposing it into voltage using the AD8220 instrumentation amplifier
I want to make a phase detection on the signal delivered by the DDS and the one measured at my DUT. I thought of using a mixer for it (the AD8343 or the LT5526)
I thought of feeding my reference signal to the RF input and the received signal from the DUT to the LO input. But i read that i should be careful to the reflexion of the LO signal on the RF and the output. So this would be my first question which filtering should i use to avoid this effect?
the output signal will finally be feed to an ADC and processed with a Micro controller to extract the phase and amplitude change.
My second question more theoretical probably, but what is the difference between a Passive mixer and an active one? Does it make a difference for sinusoidal signals?
I thank you in advance for your help and your advices :)
Best regards,