Post Go back to editing

EV-ADF4401ASD2Z Evaluation Board's output is off frequency in Translation Loop mode

Hi Community,

I am evaluating the EV-ADF4401ASD2Z Evaluation Board and seemingly can't get the RF output to stay at the desired frequency in Translation Loop Mode. In Calibration mode the output is exactly on the target. 

The settings:

  1. Calibration Ref - 10 MHz / +9 dBm.
  2. External Reference - 10 MHz / +9 dBm
  3. External LO - 4.5 GHz / 0 dBm
  4. Windows 10, 64-bit OS

The software controlling the board is ACE v. 1.24.3095.1398.

The output signal in Translation Loop Mode sits at about 4.28 GHz vs 4.51 GHz in Calibration Mode.

Power supply is 6 VDC / 800 mA  from a benchtop U8002A by Keysight.

If anyone could reply with suggestions, I'd greatly appreciate it.

Thank you.

90125



Added tag
[edited by: ggall at 3:29 PM (GMT -5) on 19 Nov 2021]
Parents Reply Children
  • I'm glad you were able to get this working.

    HMC3716 will accept a 10 MHz square wave signal, but due to filtering on the ADF4401A's IF path, the IFoutput will be severely attenuated at 10 MHz. The external reference and IF signals must match in frequency.

    For best jitter performance, it is recommended to use a higher IF frequency. See figure 18 on page 11 of the ADF4401A datasheet. IF signals between 100 MHz and 700 MHz give the best jitter performance, although this will also depend on the quality of your LO and external reference sources.