EVAL-ADF4371 board input supply range

Greetings,

The EVAL-ADF-4731 board uses two LT3045 low drop linear regulators that have an input range up 20V. The EVAL-4731 board datasheet only says to connect the board to 6V. Can the board be powered at 9V, 12, and a voltage up to 20V? Can higher power supply voltage be used when the EVAL-4371 is connected to the EVAL-SDP_CS1Z controller board that is connected to a computer via a USB cable?

Parents Reply Children
No Data