Hello,
I would like to ask you experts how to design the peripheral circuit parameters of the LT6200 for the loop filter of the ADF4401A?
Regards
HMC3716
Production
The HMC3716LP4E is a digital phase frequency detector which operates from 10 to 1300MHz. It is intended for use
in low phase noise synthesizer applications...
Datasheet
HMC3716 on Analog.com
LT6200
Production
The LT6200/LT6201 are single and dual ultralow noise, rail-to-rail input and output unity gain stable op amps that feature 0.95nV/√Hz noise voltage....
Datasheet
LT6200 on Analog.com
LT6200
Production
The LT6200/LT6201 are single and dual ultralow noise, rail-to-rail input and output unity gain stable op amps that feature 0.95nV/√Hz noise voltage....
Datasheet
LT6200 on Analog.com
Hello,
I would like to ask you experts how to design the peripheral circuit parameters of the LT6200 for the loop filter of the ADF4401A?
Regards
Hi little_rabbit: I'm not sure what filter parameters you're looking for, nor what the ADF4401A wants to see. My favorite filter is the 3rd order Butterworth shown on the back page of the LTC6240 data sheet. That's a 150kHz (-3dB) filter, but the R's and/or C's can be scaled for other frequencies.
Hi,
We are currently working on the ADISIMPLL model for ADF4401A and it will be available in ADISIMPLL soon.
Regards,
Kudret
"soon"
Is there an ETA for including ADF4401A in ADISIMPL?