The devices that we are manufacturing includes a RF detector AD8317. 10% of them fail.
The schematic is the same of Figure22 with the same value of components and CPLF=8.2pF. The RF incident signal is -40dBm CW at 27MHz.
Normally the circuits work well but in the some cases without explanation the does not work properly and output dc voltage change from 1.16VDC to 0.1VDC. The DC voltage (PIN8) INLO changes from 4.25Vdc to 1.04Vdc, the voltage PIN6 change from 0.47Vdc to 0.2Vdc and the voltage (PIN3) change from 1.22Vdc to 1.04Vdc.
Can it be an internal inestability produced by noise peak?