Hi,
What is the value of the parameter P1dB of the HMC1114PM5E ?
I do not see in the datasheet value of P1dB.
Thanks.
Best regards,
Vitaly
HMC1114PM5E
Recommended for New Designs
TThe HMC1114PM5E is a gallium nitride (GaN), broadband power amplifier delivering >10 W (up to 42 dBm) typical with up to 55% power added efficiency (PAE...
Datasheet
HMC1114PM5E on Analog.com
Hi,
What is the value of the parameter P1dB of the HMC1114PM5E ?
I do not see in the datasheet value of P1dB.
Thanks.
Best regards,
Vitaly
Hi Vitaliy063,
Here is the P1dB across freq & temperature.
Regards,
Jim B
Hi Vitaliy063,
Here is the P1dB across freq & temperature.
Regards,
Jim B
HI
How is it possible that the P1 dB of >10 W amplifier is less than 5 W at 25 deg?
Datasheet shows 42 dBm output power . Could you please provide me the information that it can deliver output greater than 10 W ???
Vitaliy063 ,
The HMC114PM5E is a GaN device. GaN has a soft compression, so, P1dB is low compared to the Saturate output power. See attached Gain vs. Pin plot.
Regards,
Jim B