Post Go back to editing

Computer Controlled Frequency Sweep Generation

Hi,

I am using ADL5920 (via DC2847A Kit) to measure S11 over 10 MHz to 20 MHz range. I am looking for a computer-controlled frequency sweep generator that can generate clean frequency sweep from 10 MHz to 20 MHz range that can be fed to ADL5920 to measure S11 over this range. It should be computer controlled so that I can sync the S11 measurements with the instantaneous frequency in my software.

I need to measure S11 over this range at 100Hz. So a fast frequency sweep generator is required. It can be an externally powered Evaluation Kit for now. It should be standalone i.e. I can't input a reference frequency to it so it should have an internal reference. 

Thank you for your response.

Parents Reply Children
No Data