Post Go back to editing

Why is the simulation of ADF4001 very different from the actual?

I am trying to use ADF4001 to synchronize a 100MHz VCXO to an external 100MHz reference signal(from a TCXO with Kv=330Hz/V), and I set the PFD at 200KHz with loop bandwidth around 445Hz.

I used ADIsimPLL to calculate the loop filter and ADI PLL Int-N to calculate the register, but I found it don't get latched.

then I try to change the PFD to 100KHz、50KHz and 25KHz with no hardware changes, then it get latched, but with a very long time.(about several hundred ms to 1s)

that's made me confused that if that's normal and if the ADIsimPLL is with guiding significance.

the attachment is the ADIsimPLL file, please help m4001e to check if there are something wrong with the hardware or register code?

the hardware maybe correct because i copied it from other 10MHz latch 100MHz project. and i checked that it's power supply is correct.


1050.ADF 4001.rar

Parents
  • Hello,

    With a very narrow loop bandwidth the PLL will take a very long time to settle. This is one of the trade offs for the narrow cutoff frequency in the loop filter. With LBW < 1kHz a settle time of 5ms or more is not unexpected. 

    In your ADIsimPLL simulation you have set the CP current for the sim = 5mA whereas you have programmed the CP current = 2.5mA which explains why the part wouldn't lock at first since with CP current = 2.5mA the loop filter you have designed could be somewhat unstable due to reduced phase margin. I would recommend changing the programmed CP current to 5mA to match closer to the sim

    Regards,

    Alex

  • Hi!
    I want to ask for help too. I previously ordered an ADF4001 PLL module and a MAX2606 oscillator module from China. I want to build an FM transmitter in the broadcast band (87.5 - 108MHz) and I would need a suitable filter between the two modules, but I don’t have enough knowledge to scale. The point would be to be as slow as possible so it is insensitive to high deflection and low frequency sound components. FM radiation uses a plus-minus 75 khz stroke. Tuning in 100khz increments.

Reply
  • Hi!
    I want to ask for help too. I previously ordered an ADF4001 PLL module and a MAX2606 oscillator module from China. I want to build an FM transmitter in the broadcast band (87.5 - 108MHz) and I would need a suitable filter between the two modules, but I don’t have enough knowledge to scale. The point would be to be as slow as possible so it is insensitive to high deflection and low frequency sound components. FM radiation uses a plus-minus 75 khz stroke. Tuning in 100khz increments.

Children
No Data