Post Go back to editing

input and output impedance matching of ADL8150

Recently I bought some ADL8150 and want to use it to amplify the signal at a single frequency 10.24GHz. However the S11 and S22 of ADL8150 is not so good whose value at 10.24GHz is -10dB and -6dB respectively.(S11: -10dB, S22:-6dB). Is the S-Parameter file that you provide tested from the evaluate-board that takes the input and output transmission lines into account? If so,  how could I remove the impact of input and output transmission lines in a smith chart to accurately match the impedance to 50Ω at 10.24GHz? Or you could just teach me how to match the input and output impedance to 50Ω at 10.24GHz so that ADL8150 could better amplify the 10.24GHz signal. I am not good at impedance matching. Look forward to your guidance and suggestions!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.