Hi, I used the HMC981LP3E for controlling bias on the HMC460LC5 Follow the circuit recommended by AN-1363,But HMC981 has no correct output.
The test results are as following:
1.VDD is 8.75V and VDIG is 5V.
2.VNEG =+0.8V,VGATE=+0.7V(The output of VGATE is a negative voltage bewteen -2 to 0V theoretically)
3.VDRIN has no output .(In fact, its test value is equal to +0.15V)
Did I do something wrong,or was there something I ignored?