Post Go back to editing

HMC8073 with Vdd=3.3V

Thread Summary

The user inquired about the HMC8073 DSA's insertion loss and attenuation range when operating at 3.3V supply voltage in the 2.6 to 3GHz frequency range. The support engineer confirmed that these parameters are not expected to change compared to the 5V supply voltage. The user thanked the engineer for the clarification.
AI Generated Content

Hi all,

I will ike to use the HMC8073 DSA in the range of 2.6 to 3GHz with a supply voltage of 3.3V.

According to the datasheet, the minimum supply voltage Vdd is 3.3V.

There is some change in the insertion loss or attenuation range with the respect to the 5V case?

Best Regards,

Santiago Calvo

Parents Reply Children
No Data