Hi,
Attached pdf document provides the layer information and silkscreen. Top and bottom layers can be seen easily and internal layers are both ground layer.
Kudret
Thanks for your relpy! Could you explain the layer tabel that I transferred from gerber file to CAM file in Altium Designer specificily? For example,what is the difference between "smd0042" ,"sm0248" and "smd0123" ,and which layer is the top layer ? "art001" or others? The screenshot of layer table has been placed in the attachment,thanks!
Hi,
Layers are as given below:
-art1, art2, art3 and art4 are the top, second, third and bottom copper layers, respectively
-dd124 is drill drawing
-sm0121 is top soldermask
-sm0428 is bottom soldermask
-sm004022 is bottom pastemask
-smd0123 is top pastemask
-sst001026 is top silkscreen
- drl01 is drill file
Regards,
Kudret
I appreciate your help very much. In addition, I would like to ask how you determine the layer type in Alutim designer,is there a universal method or the official instructions from ADI (maybe I did not find it)
Hi,
I am not familiar with Altium and not able to provide a method for you.
I guess it should be a common question and an answer can be found easily on the web.
Regards,
Kudret
thanks!