ADL5569 - amplifier 2 pin connections when not used

Hello. 

In my application I am only using one channel of the dual channel ADL5569.  Amplifier 1 is used, amplifier 2 is not.

Is it OK to no-connect (or ground?) VCC2 and all of the other amplifier 2 pins in this application? 

The datasheet seems to suggest that the two amplifiers are completely independent. Not powering an amplifier would save ~8mA.

Thanks for the help.

Parents Reply Children
No Data