ADF5902: PLL not locking for CW

Hi,

I am trying to get my PLL to lock, but have been unsuccessful in trying different register writes/loop filter configurations. My sequence/loop filter is listed below can you see any potential error with my configuration? I am able to get tones close to my signal(24.069GHz usually) but don't get a lock. I suspect it has something to do with the write sequence, I am using the ADF5902 software to manually write in the values.

Frequency=24.125GHz

REFin=19.2MHz

write sequence:

 parameter r0  = 32'h02000007;  // R7

   parameter r1  = 32'h0000002B;  // R11

   parameter r2  = 32'h0000000B;  // R11

   parameter r3  = 32'h0018000D;  // R13

   parameter r4  = 32'h1D32A64A;  // R10

   parameter r5  = 32'h2A20B929;  // R9

   parameter r6  = 32'h40003E88;  // R8

   parameter r7  = 32'h800FE520;  // R0

    // #10us

   parameter r8  = 32'h01620427;  // R7

   parameter r9  = 32'h00000006;  // R6

   parameter r10 = 32'h01E28005;  // R5

   parameter r11 = 32'h00000004;  // R4

   parameter r12 = 32'h01897803;  // R3

   parameter r13 = 32'h00020642;  // R2

   parameter r14 = 32'hFFF7FFE1;  // R1

   parameter r15 = 32'h800FE720;  // R0

    // #1200us

   parameter r16 = 32'h800FE560;  // R0

   parameter r17 = 32'h800FED60;  // R0

    // #500us

   parameter r18 = 32'h800FE5A0;  // R0

   parameter r19 = 32'h800FF5A0;  // R0

    // #500us

   parameter r20 = 32'h00000011;  // R17

   parameter r21 = 32'h00000010;  // R16

   parameter r22 = 32'h0000000D;  // R14

   parameter r23 = 32'h2800B929;  // R9

   parameter r36 = 32'h01620427;  // R7

   parameter r37 = 32'h00000006;  // R6

   parameter r38 = 32'h01E28005;  // R5

   parameter r39 = 32'h00002004;  // R4

   parameter r40 = 32'h0189F803;  // R3

   parameter r41 = 32'h801FE560;  // R0

   // #100us

   parameter r42 = 32'h0000110B;  // R11

   parameter r43 = 32'h01E28005;  // R5

Loop filter:

leveraged previous questions:

https://ez.analog.com/rf/f/q-a/546031/adf5902-pll-not-locking

https://ez.analog.com/rf/f/q-a/544087/adf5902-cannot-be-locked

Top Replies

    •  Analog Employees 
    Jul 29, 2021 +2 verified

    As  mentioned, you are missing a write to R12 to enable the charge pump current.

    The INT & FRAC settings need to be updated for your reference frequency, ref doubler & divider settings. Refer to…

Parents Reply Children
No Data