Post Go back to editing

ADF4355 - any examples of C-code for codfiguration?

Thread Summary

The user needs C-code for configuring the ADF4355 on the AD9161-FMCC-EBZ board. The evaluation software can generate register values, which can be written using a standard SPI library. The C# source code for the evaluation software is available for reference. The CE pin must be connected to 3.3V to enable the chip.
AI Generated Content

D9161Hello.

I need some tool for generating C-code for configuring ADF4355 at AD9161-FMCC-EBZ board.

Or any examples of C-code for configuring ADF4355.

I've looked ADIsim software but I've not found there any functions for generating C-code, at least register access sequences.

Is it possible to get something helpful?

My target is configuring ADF4355 at AD9162-FMCC-EBZ board in the same manner as ACE with PIC software do it.

Thank you all in advance for any help.