Post Go back to editing

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Parents on Nov 30, 2022 12:11 PM in reply to Jun2009

For DC2645A board for LTC5594:

LTC5594,Cls,D5594,01,01,DC,DC2645A,-------------

  • FormerMember
    0 FormerMember on Nov 30, 2022 1:25 PM in reply to Jun2009

    The eeprom on the DC2465A board is a MICROCHIP, 24LC025-I/ST. You can contact Microchip for help in programming. Note that the eeprom is only needed for QuikEval and not needed for normal operation of LTC5594.

  • Reply
    • FormerMember
      0 FormerMember
    on Nov 30, 2022 1:25 PM in reply to Jun2009

    The eeprom on the DC2465A board is a MICROCHIP, 24LC025-I/ST. You can contact Microchip for help in programming. Note that the eeprom is only needed for QuikEval and not needed for normal operation of LTC5594.

    Children
    No Data