LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection
LTC5594
Recommended for New Designs
The LTC5594 is a direct conversion quadrature demodulator optimized for high linearity zero-IF and low-IF receiver applications in the 300MHz to 9GHz frequency...
Datasheet
LTC5594 on Analog.com
LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection
can you help provide LTC5594 DC2645A eeprom string data like <LTC5586,Cls,D5586,01,01,DC,DC2349A,>used on LTC5586
Have you solved the problem? I got the same issue.
For DC2645A board for LTC5594:
LTC5594,Cls,D5594,01,01,DC,DC2645A,-------------
how to program the eeprom string?
how to program the eeprom string?
The eeprom on the DC2465A board is a MICROCHIP, 24LC025-I/ST. You can contact Microchip for help in programming. Note that the eeprom is only needed for QuikEval and not needed for normal operation of LTC5594.
Translation:
The character string can be written directly using the MCU
可以使用单片机直接写入字符串