Post Go back to editing

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Thread Summary

The user encountered an issue with the LTC5594 - DC2465A and DC590B boards where QuikEval could not load the module. The final solution suggested downloading and installing the module directly. The supply current should be around 470mA, and there should be no current on Vcm. The user also provided similar issues with other boards (DC2039A and DC2100B-C), and the support engineer recommended posting the question in the Power By Linear forum for further assistance. For the DC2465A EEPROM string, the correct format is: LTC5594,Cls,D5594,01,01,DC,DC2645A. The EEPROM can be programmed using an MCU.
AI Generated Content

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Parents on Nov 30, 2022 12:11 PM in reply to Jun2009
0

For DC2645A board for LTC5594:

LTC5594,Cls,D5594,01,01,DC,DC2645A,-------------

Reply
  • FormerMember
    FormerMember
on Nov 30, 2022 12:11 PM in reply to Jun2009
0

For DC2645A board for LTC5594:

LTC5594,Cls,D5594,01,01,DC,DC2645A,-------------

Children on Nov 30, 2022 1:25 PM in reply to Jun2009
0

The eeprom on the DC2465A board is a MICROCHIP, 24LC025-I/ST. You can contact Microchip for help in programming. Note that the eeprom is only needed for QuikEval and not needed for normal operation of LTC5594.

  • Translation: 

    The character string can be written directly using the MCU

    可以使用单片机直接写入字符串