LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection
LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection
Firstly, I configure the DC5990B and LTC5594 with the above instructions and quickEval shows the following results
When i click the Open button, it shows
And I will shows the two photos of the conncected board
And how can I resolve this problem?
The supply current should be about 500mA and the current on Vcm is about 7mA. Is it OK? The other connections are corret.
500mA supply current is at the upper limit. There should be no current on Vcm.
I am running into the same issue with the DC2039A board, can you please link the direct module download for that as well?
I believe this is the correct link:
https://ltspice.analog.com/quikeval/insDC2039A.msi
Thank you for the link, that worked to download the installer. I am still unclear on where/which files need to be placed to work. I can run the em4015 application directly, but get a blank grey screen. The quikeval still pops up with the same error, even with the downloaded/installed content moved to the same folder (C:/Program Files/LTC/QuikEval). Is there a step I am missing?
Here is a quick shot of what the screens look like:
Could you post your question in Power By Linear - EngineerZone (analog.com) forum?
Engineers there are most qualified to help you troubleshooting the particular problem you are facing and answer your questions on battery charge controller products.
ok, I will post there as well, it just seemed like the same QuikEval issue mentioned here so I wanted to understand the solution of where the manual installation of the files needs to go. I am still seeing a problem with QuikEval rather that the demo board itself...
I also met this problem yesterday
my demo supply voltage is 4.75 and supply current is 510 ,So is it normal ?
we found the download DLL file is 0 kb ,could you upload the DLL file directly
we found the download DLL file is 0 kb ,could you upload the DLL file directly