Post Go back to editing

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Thread Summary

The user encountered an issue with the LTC5594 - DC2465A and DC590B boards where QuikEval could not load the module. The final solution suggested downloading and installing the module directly. The supply current should be around 470mA, and there should be no current on Vcm. The user also provided similar issues with other boards (DC2039A and DC2100B-C), and the support engineer recommended posting the question in the Power By Linear forum for further assistance. For the DC2465A EEPROM string, the correct format is: LTC5594,Cls,D5594,01,01,DC,DC2645A. The EEPROM can be programmed using an MCU.
AI Generated Content

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Parents on Jul 23, 2021 12:58 PM in reply to caocheng
0

Please verify the supply voltage and current are correct. Adjust Vsupply until Vsense is 5V. The supply current should be about 470mA. Vcm should be 0.9V or floating. (Be aware that the 4 IF outputs have 0.9V common-mode voltage on them.) The jumper for Vlogic should be set to "INT" position. Make sure the DC590B's VCCIO jumper is set to 3.3V.

  • The supply current should be about 500mA and the current on Vcm is about 7mA. Is it OK? The other connections are corret.

  • FormerMember
    FormerMember on Jul 23, 2021 9:39 PM in reply to caocheng
    0

    500mA supply current is at the upper limit. There should be no current on Vcm. 

  • I am running into the same issue with the DC2039A board, can you please link the direct module download for that as well?

  • Thank you for the link, that worked to download the installer. I am still unclear on where/which files need to be placed to work. I can run the em4015 application directly, but get a blank grey screen. The quikeval still pops up with the same error, even with the downloaded/installed content moved to the same folder (C:/Program Files/LTC/QuikEval). Is there a step I am missing?

    Here is a quick shot of what the screens look like:

  • FormerMember
    FormerMember on Feb 16, 2022 3:54 PM in reply to szabom
    0

    Could you post your question in Power By Linear - EngineerZone (analog.com) forum?

    Engineers there are most qualified to help you troubleshooting the particular problem you are facing and answer your questions on battery charge controller products. 

  • ok, I will post there as well, it just seemed like the same QuikEval issue mentioned here so I wanted to understand the solution of where the manual installation of the files needs to go. I am still seeing a problem with QuikEval rather that the demo board itself...

  • I also met this problem yesterday 

  • Reply Children
    No Data