Post Go back to editing

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Thread Summary

The user encountered an issue with the LTC5594 - DC2465A and DC590B boards where QuikEval could not load the module. The final solution suggested downloading and installing the module directly. The supply current should be around 470mA, and there should be no current on Vcm. The user also provided similar issues with other boards (DC2039A and DC2100B-C), and the support engineer recommended posting the question in the Power By Linear forum for further assistance. For the DC2465A EEPROM string, the correct format is: LTC5594,Cls,D5594,01,01,DC,DC2645A. The EEPROM can be programmed using an MCU.
AI Generated Content

LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.