LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LTC5594
Recommended for New Designs
The LTC5594 is a direct conversion quadrature demodulator optimized for high linearity zero-IF and low-IF receiver applications in the 300MHz to 9GHz frequency...
Datasheet
LTC5594 on Analog.com
LTC5594 - DC2465A and DC590B show the Cannot load module for device with right connection


Firstly, I configure the DC5990B and LTC5594 with the above instructions and quickEval shows the following results

When i click the Open button, it shows

And I will shows the two photos of the conncected board


And how can I resolve this problem?
Could you try downloading and installing the module directly while we look into this issue?
Could you try downloading and installing the module directly while we look into this issue?
Is this OK ? The QVal still don't work
Please verify the supply voltage and current are correct. Adjust Vsupply until Vsense is 5V. The supply current should be about 470mA. Vcm should be 0.9V or floating. (Be aware that the 4 IF outputs have 0.9V common-mode voltage on them.) The jumper for Vlogic should be set to "INT" position. Make sure the DC590B's VCCIO jumper is set to 3.3V.
The supply current should be about 500mA and the current on Vcm is about 7mA. Is it OK? The other connections are corret.
500mA supply current is at the upper limit. There should be no current on Vcm.
I am running into the same issue with the DC2039A board, can you please link the direct module download for that as well?
I believe this is the correct link:
https://ltspice.analog.com/quikeval/insDC2039A.msi
Thank you for the link, that worked to download the installer. I am still unclear on where/which files need to be placed to work. I can run the em4015 application directly, but get a blank grey screen. The quikeval still pops up with the same error, even with the downloaded/installed content moved to the same folder (C:/Program Files/LTC/QuikEval). Is there a step I am missing?
Here is a quick shot of what the screens look like:

Could you post your question in Power By Linear - EngineerZone (analog.com) forum?
Engineers there are most qualified to help you troubleshooting the particular problem you are facing and answer your questions on battery charge controller products.
ok, I will post there as well, it just seemed like the same QuikEval issue mentioned here so I wanted to understand the solution of where the manual installation of the files needs to go. I am still seeing a problem with QuikEval rather that the demo board itself...