Post Go back to editing

HMC832 Frequency hopping method...

Dear Professional!

I'm using HMC832, actually it is nice to generate 800M to 1GHz. But it is slow to do auto-calibration ever time. So I'm trying to use frequency hopping method. I'm trying to do calibration one time and setting VCO tune register value after 0x03, 0x04 register setting. But I'm curious of the reading value of 0x10 register. The 0x10[8] =0, it means that the auto calibration is not busy, and reading is 0xBA for all over the frequencies. Is it correct to read all the same 0xBA values all over 100 frequencies? or it should be changed as the every frequencies?

Regards, nsyun!

Parents Reply Children
No Data