Can demorad projects be transplanted to tinyrad?

Hi ADI engineers

I get a project based on demorad platform. But ADI recommends using tinyrad replace demorad.

Could the demorad project be transplanted to tinyrad directly?

Thanks

  • +1
    •  Analog Employees 
    on Jul 27, 2021 10:22 AM

    TinyRad and DemoRad are fairly comparable since they both use the same RF chipset. The TinyRad is preferred as it is a smaller package and it can run off 5V USB power. We implemented new firmware on TinyRad to fix the sample rate which allows the ramp timings to be customized. It is possible to upgrade the DemoRad to run from the TinyRad version of the software. This requires a minor hardware change (resistor) and a Firmware upgrade. 
    If you would like access to the custom ramp timings, as per UG-1709, then let me know and I can email details to you