ADIsimPLL 5.30.02 CSV output precision bug

I've been playing with the EV-RADAR-MMIC2 FMCW radar chipset using ADIsimPLL (ADR4159, ADF5901, ADF5904), and would like to do some post-processing on the ramp output. I find in the TimeDomain tab that I can right-click on the ramp graph and save the data to a CSV file. However, the frequency precision in that output file is no better than 100kHz. If I turn on a marker for that graph, it shows values down to 1Hz.

Similarly, the time step precision in the output CSV file is rather coarser than the data, with many values repeated on adjacent lines.

Can you please fix this so the CSV output has as much precision as is used internally?

Thanks!