Hi.
I would like to know a low noise driver that can be connected to ADF5904 output without loading the ADF5904 output stage.
The driver output will be connected to ADC.
The driver specs required are Gain >10dB, 3dB Bandwidth > 10MHz and the ADC will be having input impedance of 10K.
We were using the ADA4940-2 as the output driver for our use case, with resistors RG and RF of 1K and 10K respectively for gain of 20dB.
But the output is affected by noise.
If we reduce the resistors around 200 ohms and 2K respectively, the output of ADF5904 will get loaded as the output impedance of ADF5904 is 900Ohm differential, so 450Ohm single ended.
Please let me know which output driver can be used.
Preferable two amplifiers in a single chip.
Thanks,
Sutej.