Dear Sir,
In ADI web site gerber file of HMC907APM5E has assigned as HMC994. COuld you please share HMC907APM5E eval board (represented in datasheet) wtih us? Thanks...
HMC907APM5E
Production
The HMC907APM5E is a GaAs MMIC pHEMT Distributed Power Amplifier which operates between 0.2 and 22 GHz. This self-biased power amplifier provides 14 dB...
Datasheet
HMC907APM5E on Analog.com
HMC994
Obsolete
The HMC994 devices are GaAs, monolithic microwave integrated circuit (MMIC), PHEMT distributed power amplifiers which operate between dc and 28 GHz or...
Datasheet
HMC994 on Analog.com
Dear Sir,
In ADI web site gerber file of HMC907APM5E has assigned as HMC994. COuld you please share HMC907APM5E eval board (represented in datasheet) wtih us? Thanks...
Hello Dan02,
If you investigate in excel file, the IC is HMC994 not HMC907. Also, the layout is compatible for HMC994. HMC907 has not either a VGG pin or a VDD pin.
Thanks,
Hello Dan02,
If you investigate in excel file, the IC is HMC994 not HMC907. Also, the layout is compatible for HMC994. HMC907 has not either a VGG pin or a VDD pin.
Thanks,
Hi robotech,
They use the same board. They both have a VGG pin. VDD is applied through a bias tee on the HMC994, just like the HMC907.
Thanks,
DanO