Post Go back to editing

ADF4372 Lock Detect

I want to implement analog lock detect on the ADF4372.  I have read AN-873 regarding lock detect behavior on ADF4xxx PLLs.  On page 19 of the datasheet, it shows that analog lock detect is available at the MUXOUT pin when properly programmed.  On page 32 of ]he datasheet, in REG0020, for the list of MUXOUT configuration bits [7:4], digital lock detect is 0001...but there is no entry for analog lock detect.  What is the correct bit sequence?  Thanks.

Parents
  • Hi,

    AN-873 does not include ADF4371, please see appendix for applicable parts.

    Analog lock detect is not a function that is implemented with ADF4372 and should not be given the datasheet. You can use digital lock detect instead. Is there any special requirement for you to use analog lock detect? 

    Kudret

  • Then the datasheet has some errata.

    Table 5 on page 10 for pin 41 of the ADF4372 datasgeet, listing MUXOUT functions, lists analog lock detect as one of the options.

    Figure 32 on page 19 of the ADF4372 datasheet shows analog lock detect as one of the options.

    Based on that, analog lock detect seemed available.  I had decided to use it since I'm doing some fast manipulation of the part, but I can switch over to digital lock detect with some reduction in functionality.

Reply
  • Then the datasheet has some errata.

    Table 5 on page 10 for pin 41 of the ADF4372 datasgeet, listing MUXOUT functions, lists analog lock detect as one of the options.

    Figure 32 on page 19 of the ADF4372 datasheet shows analog lock detect as one of the options.

    Based on that, analog lock detect seemed available.  I had decided to use it since I'm doing some fast manipulation of the part, but I can switch over to digital lock detect with some reduction in functionality.

Children