What is the output saturated power level for this gain block? What input power level to drive this at the output saturation power level?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
HMC311LP3
Last Time Ship
The HMC311LP3(E) is a GaAs InGaP Heterojunction Bipolar Transistor (HBT) Gain Block MMIC SMT DC to 6 GHz amplifiers. This 3 × 3mm QFN packaged amplifier...
Datasheet
HMC311LP3 on Analog.com
What is the output saturated power level for this gain block? What input power level to drive this at the output saturation power level?
There are two compression plots in the datasheet on the third page at 1 GHz and 6 GHz. The trace does not quite reach full saturation but I would say that from these plots you are looking at Psat levels of 17.5 dBm (1GHz) and 14 dBm (6GHz). So the delta between OP1dB and Psat is somewhere between 1.5 dB an 2 dB. The corresponding input levels to get to saturation would be approx +9 dBm (1GHz) and +6 dBm (6GHz).