Post Go back to editing

AD8310 - Possible Output Integrity Issue

Thread Summary

The user is experiencing noise and instability issues with the AD8310 output voltage during frequency sweeps in a scalar network analyzer. The problem was identified as RF interference from cell phone signals, particularly when switching between Wi-Fi and 4G. Solutions include using a 5-60 MHz bandpass filter, shielding the input leads, and configuring the AD8310 for differential input to improve noise rejection.
AI Generated Content

Hi everyone,
Some time ago I started building my own scalar network analyzer. I already got some great help from Bruce_H on this forum so far for which I am very greatful! Do note that I am not a professional electrical engineer when answering/suggesting, but a chemist-turned-electronics-hobbyist, haha.


The main idea of my board is as follows:

AD9851 DDS chip outputs a sine wave with programmable frequency (5 - 60 MHz). This is passed through and LPF to a buffer amplifier which in turn sends it to a quartz crystal to assess its resonance frequency. I measure the envelope of the sine wave that passes through the quartz crystal using an AD8310 in single-ended configuration. The output is again buffered by an opamp to be sent to the microcontroller ADC to measure the voltage. I use python as my DAQ platform and to control the frequency programming over usb.

Thus far I can see that it works mostly as expected. However, I still have some issues related to noise. When I try to pinpoint the origin of the noise I can at least see that something strange is happening at the AD8310 output. During my frequency sweeps for some frequencies the AD8310 output voltage suddenly drops seemingly out of nowhere.. I know this is not much to go on, considering the full scope of the project but I was wondering if someone has had any similar issues? Most of the time it works just fine, but every once in a while it seems ot run into this instability. Could it be the AD8310 or do you suspect something else?

I posted an image of what it looks like in my DAQ software below. I would really appreciate some help/input.

If you require additional information or have ideas of what I could probe with my scope, please let me know!

Cheers,
Rens

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.