Post Go back to editing

LTC5586 : Anti-alias Lowpass Filter

Hello

I would like to have more informations about I/Q anti-alias Lowpass filter for LTC5586 IQ demodulator.

I don't understand how to calculate/simulate Low pass filter defined in datasheet page 24 ?

When I try to simulate, with LTspice this filter (page34), Bode diagram is not flat with several resonances.

Could you send me how this filter can be simulate with ltspice?

Thanks

Best regards

BP_FRANCE

Parents
  • FormerMember
    0 FormerMember
on Mar 30, 2021 4:34 PM

Maybe the attached LTspice example would help you. Although it is for LTC5594, the LTC5586's IF output is the same. Note only half of the differential output is shown. The parallel resistance R3//R7 sets the output impedance seen by the ADC. In this case, 68.1//200 = 50 ohms, single-ended (we are interfacing to an ADC with 100 ohm differential input impedance. The anti-alias filter has asymmetrical impedance: 68.1 ohms at the input and 200//50 = 40 ohms at the output.

 LTC5594 Anti-alias filter 500MHz.asc

Reply
  • FormerMember
    0 FormerMember
on Mar 30, 2021 4:34 PM

Maybe the attached LTspice example would help you. Although it is for LTC5594, the LTC5586's IF output is the same. Note only half of the differential output is shown. The parallel resistance R3//R7 sets the output impedance seen by the ADC. In this case, 68.1//200 = 50 ohms, single-ended (we are interfacing to an ADC with 100 ohm differential input impedance. The anti-alias filter has asymmetrical impedance: 68.1 ohms at the input and 200//50 = 40 ohms at the output.

 LTC5594 Anti-alias filter 500MHz.asc

Children
No Data