Post Go back to editing

Analog Band Pass Tunable Filters (ADMV8420,ADMV8416,HMC892A,HMC891A)

Thread Summary

The user seeks a high-speed, low-noise control circuit for Vcnt pins of Analog Band Pass Tunable Filters (ADMV8420, ADMV8416, HMC892A, HMC891A) to avoid degrading LO phase noise. A recommended solution uses the AD5760 DAC and ADA4898 op-amp, achieving a baseband noise spectral density of 10nV/rtHz and a tuning speed of 1usec. The user has implemented a similar setup with AD9708ARUZ and ADA4898, adding an in-the-loop correction for front glitches.
AI Generated Content

Dear All!

I'm going to use Analog Band Pass Tunable Filters (ADMV8420,ADMV8416,HMC892A,HMC891A) for DDS base LO.

Unfortunately the specifications do not provide any typical schematic or circuit  for manage Vcnt control Pin's.

The main idea is to control the bandpass filters by DAC with OP AMP with the higher update rate  up to 200 ns settling time, without reducing the LO phase noise performance.

In my opinion the Vcnt pins are very sensitivity to noise, and If you can provide me some high frequency low noise application circuits to do it I will be apparated.    

Thanks in advance

Aram Khachatryan