Post Go back to editing

operation of ADL5375

Hello,

I have a question regarding the operation of ADL5375. Based on the datasheet, my understanding is that the ADL5375 evaluation board can only be operated in differential mode with a common mode bias of 500 mV or 1500 mV. Are there options to operate this board without this bias or in single ended mode? If this is not possible for ADL5375 , are there other IQ modulator boards that can achieve this? I am interested in a modulator with a IF bandwidth of at least DC-100 MHz and a RF bandwidth covering 500 MHz to 1500 MHz.

Thank you in advance!

Parents Reply Children
No Data