I am currently evaluating an ADAR1000-EVALZ board, and I am having issues addressing with with the evaluation software and an SDP-S (this is a precursor to using 4 daisy-chained together). I seem to be able to change the address on the ADAR using P10. For instance, I can control the board when AD1 and AD0 are low with no issue and setting either high by connecting pins 3 and 4 to 5 and 6 prevents the software from interfacing with it. However, all attempts to address the ADAR when the address is not set to zero have failed. I have tried setting both the ADDR0/1 values in the connection and GPIO tabs to match the jumper positions with no success, and ensuring the settings are correct before connecting the software to the SDP-S has not made a difference. Where might I be going wrong? I am using the default maximum gain settings text file and uploading it to the ADAR1000 using the manual register write tab. Any advice would be greatly appreciated.