Post Go back to editing

HMC1082LP4E

Hi,

1)  is the HMC1082LP4E Gain vs Temperature performance data given in the datasheet  obtained with the temperature compensation network ? 

2 ) can you suggest an opamp for the compensation network?

thank you. 

best regards 

Ali Tevfik Dengizek

Parents
  • Hi DNGZK,

    1). Is the HMC1082LP4E Gain vs Temperature performance data given in the datasheet  obtained with the temperature compensation network ?

    There is no on chip compensation network for gain vs. temp.

    The Vdet and Vref pins are a separate power detector circuit that has no impact on the gain levels. It is used to have a DC voltage measurement track the RF output power of the circuit. Yes, these can be left open if not used.

     

    2). Can you suggest an opamp for the temp compensation network?

    I would suggest the AD8531 or AD8541.

    Thanks,

    DanO

Reply
  • Hi DNGZK,

    1). Is the HMC1082LP4E Gain vs Temperature performance data given in the datasheet  obtained with the temperature compensation network ?

    There is no on chip compensation network for gain vs. temp.

    The Vdet and Vref pins are a separate power detector circuit that has no impact on the gain levels. It is used to have a DC voltage measurement track the RF output power of the circuit. Yes, these can be left open if not used.

     

    2). Can you suggest an opamp for the temp compensation network?

    I would suggest the AD8531 or AD8541.

    Thanks,

    DanO

Children
No Data