Hi all,
Our customer will develop the low frequency down converter.
RF input : 400kHz~100MHz
IF output : 100kHz
Q1:
For example, can AD831 and AD8343 be used for applications in such a low frequency range?
The input range is from 0Hz.
Q2:
For example, can A and B be used for applications in such a low frequency range?
The input range is from 0Hz.
Best regards,
sss
If it is available, can you give me advice, materials, etc. on how to design the matching circuit of the input / output circuit, precautions, etc.?