Post Go back to editing

ADL5324 Datasheet

Hi,

In the ADL5324 datasheet there are reference designs and layouts.

On page 19, figure 17, the layout for the 3500-3700MHz operation. There is a series inductor on the output, L2.

It is 4.7nH.

At 3500MHz, this gives a reactance of 103 ohms.

Considering the output impedance is 50 ohms, this will attenuate the output signal somewhat....

Am I correct?

If so what value should this be?

Best regards,

Roger.

Parents
  • Hi Rog,

                    the ADL5324 is not internally matched to 50 ohms. This impedance is 6 ohms or so and must be externally matched to 50 ohms. L2 & C2 work with the internal impedance of the ADL5324 to create a 50 ohm match for the ADL5324. The value for L2 is correct and has been tested.

    Regards,

    Jim B

  • Hi Jim,

    Ok, yes I see the S21 is 5.6 ohms and needs to be matched to 50.

    I am also trying to simulate this, but I cannot get it to match to 50.

    Do you have any spice or ADS simulation files on this device, I could then see how I am going wrong.

    Best regards,

    Roger.

  • Hi Rog,

                 On the web, we have an S-Parameter file you can download and use with ADS. I generally use a smith chart program to get a basic match at the center frequency of the band. I then use ideal components and tune function to get the desired gain and match across the band. I then substitute real components in ADS and adjust as needed to keep my gain and match. I then build and test. One point, I found at the higher freqs there is an error in the s2p file and my actual circuit is off by 250 MHz when tested. SO I offset the simulation freq and rematch in that case. I have never had to do more than 2 iterations to correct for the offset in frequency that may or may not occur.

    Regards,

    Jim B

  • Hi Jim,

    Yes I have the S parameters file, am using it in ADS.

    I have tried placing in substitution vales for the reactive components - without any success in matching it.

    I still believe the inductor is too high a value. Would you be able to check you results, for the 3500-3700 MHz band.

    Best regards,

    Roger.

  • Hi Rog,

                 I have limited data for the ADL5324 at 3500-3700 MHz. Attached is a scalar gain plot. Gain in the band is ~ 12 dB.

    Regards,

    Jim B

    PDF

  • Hi Jim,

    Thanks for that.

    This is the gain I was hoping for, however I do not get close to that.

    What is the matching network associated with that gain?

    Cheers,

    Rog.

  • Hi Roger,

                       The network is the one given in the data sheet. Are you using the exact components specified for C1, C2, C3 and L2,(Labeled as R2 in the table and on the board)

    Regards,

    Jim B

    PDF

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.