Post Go back to editing

HMC778 RFOUT coupling cap (why 100 pF)?

Hello ADI,

Why was a 100 pF coupling cap used on the HMC778 RFOUT on the eval board schematic?  Since this part operates around 10 GHz I would have expected that a much smaller coupling cap would be used.  I swept a 100 pF, C0G 0402 cap at 10 GHz and the insertion loss = 0.6 dB and the return loss = 13.5 dB.  Does ADI want the coupling cap to work down below 1 GHz for some reason?

Thanks,

Eric

Parents Reply
  • fc  100 pF 1 pF Delta
    GHz dBm dBm dB
    10.0 9.59 10.12 0.53
    10.1 9.63 10.12 0.49
    10.2 9.41 9.90 0.49
    10.3 8.36 8.83 0.47
    10.4 7.63 8.09 0.46
    10.5 7.52 8.03 0.51

    The previous data was not recorded properly.  The table above is corrected data showing output power with a 100pF and 1pF coupling cap.  Notice the dB delta is now about 0.5dB as expected.

Children
No Data