I am having a problem with a phased array board equipped with ADAR1000 and ADTR1107, which will not stop oscillating unless the front-end gain is reduced by at least 15dB from the maximum. The reason for the oscillation is that the layout design of the board is very poor and the isolation between the RFIO and PA output is not achieved, but could you please advise me on the gain setting of the ADAR1000.The oscillation stops when the 15dB ATT is used and the VGA gain is set to MAX (set value = 127), but oscillation occurs when the VGA gain is lowered by 15dB (set value = 13) without using the 15dB ATT. Is there any possible cause for this ,or should I not use the VGA with extremely low gain?