I'm looking for the junction-to-case thermal resistance of LTC5508ESC6#PBF. Thanks-
LTC5508
Production
The LTC5508 is an RF power detector for RF applications operating in the 300MHz to 7GHz range. A temperature compensated Schottky diode peak detector and...
Datasheet
LTC5508 on Analog.com
I'm looking for the junction-to-case thermal resistance of LTC5508ESC6#PBF. Thanks-
Hi SuzanneR,
Sorry, we don't have that info readily available. Note, however, Pd = 6V max * 0.85mA max = 5.1mW is very small. The device could dissipate up to an additional 8mW driving a 2mA load. This makes total dissipation = 13mW max.
Reference datasheet page 2, Theta jcn-ambient = 256 degC/W. Theta jcn-case will be less. But even with no other heat sinking (just soldered on a board), Temperature rise = 0.013W * 256 degC/W = 3.3 deg C, not a very large number.
Hope that helps! -Bruce H.
Hi SuzanneR,
Sorry, we don't have that info readily available. Note, however, Pd = 6V max * 0.85mA max = 5.1mW is very small. The device could dissipate up to an additional 8mW driving a 2mA load. This makes total dissipation = 13mW max.
Reference datasheet page 2, Theta jcn-ambient = 256 degC/W. Theta jcn-case will be less. But even with no other heat sinking (just soldered on a board), Temperature rise = 0.013W * 256 degC/W = 3.3 deg C, not a very large number.
Hope that helps! -Bruce H.