Post Go back to editing

S parameter (300kHz-12GHz)

Hi there,

I'm looking for S-parameter for parts below.

HMC998APM5E, HMC797APM5E, HMC465LP5, HMC5805A, HMC930, HMC460LC5 HMC459 

Although the freq response for some of the parts stated supporting 0-20GHz, but in the S-parameter file only have data showing from 0.01GHz.

Could you hep to confirm if these parts are tested and is it capable as low as 300KHz?

Parents Reply
  • Thanks for your response Bruce :)

    Do you have any advise on the power detector circuit?

    Forgot to mention, we are looking for a power detector that has a dynamic range of <62dB. That makes it very hard for the likes of LTC5532 and LTC5564 to meet our requirements. That is the reason why the SDLVA looked so promising to us, high dynamic range, wide frequency bandwidth, as we are also avoiding to split the detector circuits to LF and HF due to board footprint considerations. Please let us know more info on the SDLVA and its application. We will only split the circuit into LF and HF as a last resort. 

Children
No Data