Post Go back to editing

S parameter (300kHz-12GHz)

Hi there,

I'm looking for S-parameter for parts below.

HMC998APM5E, HMC797APM5E, HMC465LP5, HMC5805A, HMC930, HMC460LC5 HMC459 

Although the freq response for some of the parts stated supporting 0-20GHz, but in the S-parameter file only have data showing from 0.01GHz.

Could you hep to confirm if these parts are tested and is it capable as low as 300KHz?

Parents
  • Hi Carmen,

                      HMC465LP5 has 30 KHz to 9 GHz S-Par data. Bottom of the first TPC page.

    HMC998APM5E has 100 KHz to 9 GHz S-Par data. Top of the first TPC page.

    HMC930A-DIe has 30KHz to 3 GHz S-Par data. Fig 11.

    HMC460LC5 has 30 KHz to 1GHz S-Par data. Bottom of the first TPC page.

     HMC459-DIE has 30 KHz to 9 GHz S-Par data. Bottom of the first TPC page.

    HMC797APM5E, HMC5805A, have nothing internal that would prevent operation down to dc. But were not measured at the lower frequency band.

  •  HMC465LP5- All 3 files are starting with 0.05GHz to 25.999GHz. Please help advise what did i miss?

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.